AKD Setup Wizard
- The EtherCAT Scan and Association has been performed.
- Your project is compliant with the physical devices on the EtherCAT network.
- You have activated the Online Configuration mode in the EtherCAT Toolbar.
You then have access to the AKD parameters that are used when the drive is running.
Figure 4-28: AKD Setup Wizard